Breadcrumbs
Product Description
FactoryTalk Analytics for Devices
FactoryTalk® Analytics for Devices is an all-in-one approach to finding and reducing operational and maintenance issues. With a simple set-up, and a modern and natural interface, users are able to start identifying issues within about 5 minutes of connecting the appliance to their automation network. New and enhanced analytics are delivered regularly through a seamless synchronization approach that makes it easy to stay on top of what’s happening in an industrial environment.
FactoryTalk Analytics for Devices is an information appliance that can be deployed inside an automation network to automatically discover and analyze problems with devices that are a part of the operation. All you need is power and an Ethernet network, with one or more Ethernet/IP devices on it. Powered by embedded analytic technology and Aware Automation™, and enhanced with Shelby, a friendly chat bot, interactive Action Cards, and future connectivity to FactoryTalk VantagePoint, FactoryTalk Historian, or the FactoryTalk Cloud, FactoryTalk Analytics for Devices is a starting point, and a platform, for the Industrial Internet of Things.