Breadcrumbs
Product Description
FactoryTalk TeamONE
App for team collaboration in context with plant floor information.
FactoryTalk TeamONE is an app platform that delivers frictionless productivity for every industrial worker. The iOS and Android app is a platform and we’ve innovated to put the platform within the app itself, which reduces the friction to value to literally zero. FactoryTalk TeamONE can be downloaded, installed and used right away by anyone on company or personally owned devices. FactoryTalk TeamONE delivers the ability for your team to collaborate in context with automation device data and is tailored for industrial environments by way of not requiring any servers or even cloud/WiFi infrastructure initially, provides industrial specific features called modules, adjusts for varying levels of connectivity and opportunistically expands in value when your company chooses to connect their enterprise. FactoryTalk TeamONE can be downloaded for free from both the Apple and Google App Stores. FactoryTalk TeamOne Standard Edition is a per user email subscription enables additional modules and features. Current FactoryTalk TeamOne Standard provides all of that in the free edition plus an Alarm module.