text.skipToContent text.skipToNavigation
...

Percorso di navigazione

Compute Module Linux Red Hat

The Connected Enterprise™®

Descrizione prodotto

Compute Module Linux Red Hat

ControlLogix Compute module is chassis-based module that let you communicate directly with a ControlLogix 5570 or ControlLogix 5580 controller via the system backplane and over a network. The module offers Red Hat Enterprise Linux as embedded operating system (OS) that lets you create custom applications.

  • Include assistenza per Studio 5000
  • RSLogix
  • View Studio e include l'accesso alle Attivazioni temporanee