text.skipToContent text.skipToNavigation
...

Mensagens

FactoryTalk Analytics GuardianAI

Connected Enterprise™

Descrição do produto

FactoryTalk Analytics GuardianAI

FactoryTalk Analytics GuardianAI is an asset health monitoring application that runs at the edge. It leverages AI to provide predictive maintenance insights that help users reduce unplanned downtime and optimize maintenance planning.

FactoryTalk Analytics GuardianAI was designed with the maintenance engineer in mind. It uses data from the plant's existing variable frequency drives to monitor the behavior of plant assets such as pumps, fans, and blowers. When a deviation from normal operating behavior is detected, FactoryTalk Analytics GuardianAI will notify the user so maintenance can be planned to prevent an equipment failure. FactoryTalk Analytics GuardianAI provides premier integration with PowerFlex 755, 755T, and 6000T drives.

  • Inclui suporte para Studio 5000
  • RSLogix
  • Exibe Studio e inclui acesso a ativações temporárias