text.skipToContent text.skipToNavigation

面包屑导航

Compute Module Linux Red Hat Support and Maintenance Contract

互联企业™

产品描述

Compute Module Linux Red Hat Support and Maintenance Contract

ControlLogix Compute module with Red Hat operating system is purchased via SAP. In order to work with the module, users need to purchase also the Support and Maintenance contract here, enabling the access to updates and support for the module.

  • 包括 Studio 5000 支持
  • RSLogix
  • View Studio 并包括临时激活访问权限