text.skipToContent text.skipToNavigation

面包屑导航

RSLinx Classic

Connected Enterprise™

产品描述

RSLinx Classic

RSLinx Classic permits 3rd-party software to access data from Rockwell Automation controllers using OPC DA or DDE interface. The software is well suited to work with older software and systems containing older hardware and networks.

RSLinx Classic is a scalable offering purchased based on the need to interface with a single controller or multiple controllers, local or remote OPC clients, and the ability to pass / bridge communications between RSLinx Classic on different workstations.

  • 包括 Studio 5000 支持
  • RSLogix
  • View Studio 并包括临时激活访问权限