text.skipToContent text.skipToNavigation

추적성

저희 시스템은 4월 18일(토) 오후 8시(CDT)부터 4월 19일(일) 오전 8시(CDT)까지 계획된 유지보수 작업을 진행할 예정입니다.
이 기간 동안 기다려 주셔서 감사합니다.

ThinManager + FactoryTalk View SE Subscription

Connected Enterprise™

제품 설명

ThinManager + FactoryTalk View SE Subscription

FactoryTalk View SE, ThinManager and PinPoint together deliver a full visualization solution for production operations.

This software bundle provides everything you need to run a managed HMI visualization system. Included in the bundle is an HMI server with unlimited displays, client stations, managed thin client licenses, automated tag navigation licenses and unlimited browser-based HTML client connections.

  • Studio 5000에 대한 지원 포함
  • RSLogix
  • View Studio 및 임시 활성화에 대한 액세스 포함